2016-09-06 01:53 AM
Hello,
I'm trying to program my application to user flash memory (0x08000000) via the DFU mode with the embedded bootloader. However, the application is always programmed incompletely. See the attached picture.There is still some data after 0x0800A807 like below ( captured from the .hex file ).:10A804001838F1071CF7068000F8C61850F1001C30:10A81400F2020888611CF201021C62011CFD02D1D3:10A824000431548204A8613C92071CF20A801C2162:10A8340015921250A2041CF20A021CF20A201CF205:10A8440006401C4E0848038312008C79B04E084819:10A8540003F1071C83000854294C920654F30600A4:10A86400101CFA0100A0A20A1CF20A101CFA0640ED:10A874004C460018E102711CF20A0454F206201C32:10A88400FA0508BC611CFD082C03FE0A08EC04460A:10A8940008DCE1027550F107C4861034D30100A826......I am using STM32L486. Has anybody already got this problem? or has some idea about this?Thanks in advance.2016-09-06 04:29 AM
2016-09-06 06:59 AM
Hi vovk.dmitriy,
As a start, I recommend to check the'' Getting started with DfuSe USB device firmware upgrade STMicroelectronics extension'' and download
-Hannibal-2016-09-06 07:43 PM
Thanks, clive.
I did re-generate the HEX from the DFU. The new HEX looks same as the original one.I found this problem when I am trying to upgrade my own boot program via the embedded bootloader. I also found another strange thing is sometimes the embedded bootloader can't upgrade my application program starting from 0x08010000. The reason looks same that verification failed. But my own bootloader can do this!The following words are from section 5 of UM1879: STM32L4 Discovery kit manual. Not sure whether this could be the root cause.The following limitations exist in the bootloader V 9.0:
1. RAM data get corrupted when written via USART/SPI/I2C/USB interface
Description:
Data write operation into RAM space via USART, SPI, I²C bus or USB results in wrong
or no data written.
Workaround:
To correct the issue of wrong write into RAM, download STSW-STM32158 bootloader
V 9.0 patch package from www.st.com and load ''Bootloader V9.0 SRAM patch'' to the
MCU, following the information in readme.txt file available in the package.
2016-09-06 11:46 PM
Found the root cause in section 46 of AN2606:
For memory write operations using DFU interface:
If the buffer size is larger than 256 bytes and not
multiple of 8 bytes, the write memory operation
result is corrupted.
Workaround: if the file size is larger than 256
bytes, add byte padding to align it on 8-bytes
multiple size.
Write in SRAM is corrupted.After manually aligning the HEX on 8-bytes before generating the DFU, then DFU upgrade succeeds.
2016-09-15 01:39 AM
Hi xu.ross,
Thans for sharing your finding. -Hannibal-