2015-01-17 04:27 AM
I have just started my adventures with STM32f407 Discovery board. I'm using latest stable release of CoIDE and using up to date toolchain/libraries.
I managed to write the following code in order to use USART1 from the board
int main(void)
{
GPIO_InitTypeDef GPIO_InitStructure; // Definicja struktury do inicjalizacji PINOW
USART_InitTypeDef USART_InitStructure;
// Initialize pins as alternating function
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1);
// Modify USART_InitStructure for non -default values , e.g.
// USART_InitStructure.USART_BaudRate = 38400;
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Tx|USART_Mode_Rx;
USART_Init(USART1 ,&USART_InitStructure);
USART_Cmd(USART1 , ENABLE);
while(1)
{
while (USART_GetFlagStatus(USART1 , USART_FLAG_TXE) == RESET);
USART1 ->DR = (uint16_t)(45 & 0x01FF);
Delay(0x3FFFFF);
}
}
And as you can see on the attached picture I'm receiving incorrect data. Bascially if I change value sent the characters on the console are the same.
I have defined settings for clock configuration and confirmed it is working fine
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t)8000000) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */
/************************* PLL Parameters *************************************/
/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */
#define PLL_M 8
#define PLL_N 336
/* SYSCLK = PLL_VCO / PLL_P */
#define PLL_P 2
/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */
#define PLL_Q 7
/******************************************************************************/
Now in order to find the root cause I have tried to configure USART3 and this one works out of the box.
int main( void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* Enable GPIO clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
/* Enable UART clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* Connect PXx to USARTx_Tx*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3);
/* Connect PXx to USARTx_Rx*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3);
/* Configure USART Tx as alternate function */
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Configure USART Rx as alternate function */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_Init(GPIOC, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* USART configuration */
USART_Init(USART3, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART3, ENABLE);
SysTick_Config(SystemCoreClock / 1000);
while(1)
{
for (int var = 45; var < 128; var++)
{
USART_SendData(USART3, var);
Delay_SysTick(500); // 1 sek
}
}
}
Can anyone point me to some possible root causes ? I have already tried multiple baud rates on PC terminal / different USB<>RS232 (mostly FT232RL chips ) and slowly running out of any ideas.
Regards
Rafal
2015-01-17 05:11 AM
2015-01-17 05:28 AM
Thanks Clive for pointout. I have found your previous reply now under [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/Help%20with%20GPIO%20on%20STM32F4%20discovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=956]here
However is this somehow document for beginners ?2015-01-17 05:54 AM
2015-01-17 06:19 AM
If I may just ask on this one. Looking at the table from user manual (from beginner perspective ) I have Main function / Alternate function and board function. And in this particular example PA9 (USART1 TX) has board function of ''VBUS'' and ''GREEN LED''.
So would this be correct If I would say I cannot use alternate function if there is a board function assigned to it ?2015-01-17 07:25 AM
Unfortunately ''beginner'' is a bit vague, I'm assuming you're not three, and bring some life skills to the party. Do you have experience with electronics, microprocessors, software, try to provide some context.
You'd want to focus on the ''Free I/O'' pins, the other pins are connected to other things, and so you'd need to review the circuit, attached components, and decide if the current configuration would interfere with other uses, or if you need to remove the components. The STM32F4-DISCO has quite a lot of external circuitry, for access to more pins/functions consider a more basic breakout board configuration,.2015-01-18 02:31 PM
/* Includes ------------------------------------------------------------------*/
#include ''stm32f4xx.h''
#include <stm32f4xx_usart.h> #include <stdio.h> #include <string.h> #include <uart4.h>/*******************************************************************************
* Function Name : UART4_Configuration * Description : Configure UART4 * Input : PC10 = TX * Output : PC11 = RX * Return : None * Attention : UART connected to APB1; GPIOC connected to AHB1 * : The library does'nt handles te UART and USART different * DD4DA *******************************************************************************/ void UART4Init ( uint32_t baudrate ) { GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // this is used to configure the NVIC (nested vector interrupt controller)RCC_APB1PeriphClockCmd ( RCC_APB1Periph_UART4, ENABLE ); // UART4 is connect to APB1
RCC_AHB1PeriphClockCmd ( RCC_AHB1Periph_GPIOC, ENABLE ); // UART4 used Port-C, Pin10 as TXD,Pin11 as RXD GPIO_DeInit ( GPIOC ); // RESET CMD TO GPIOC - ob das ne gute idee ist// UART4_TX -> PC10 , UART4_RX -> PC11
GPIO_StructInit ( &GPIO_InitStructure );GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; // GPIO Pin10 (TxD) und Pin11(RxD)
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; // GPIO in Alternate Function mode GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz; // SlewRate GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // PushPullGPIO_Init ( GPIOC, &GPIO_InitStructure ); // GPIOC
// Connect UART4 pins to GPIOC
GPIO_PinAFConfig ( GPIOC, GPIO_PinSource10, GPIO_AF_UART4 ); // Alternate Function von GPIOC, Pin 10 an UART4 TX mappen GPIO_PinAFConfig ( GPIOC, GPIO_PinSource11, GPIO_AF_UART4 ); // Alternate Function von GPIOC, Pin 11 an UART4 RX mappen USART_StructInit ( &USART_InitStructure );USART_InitStructure.USART_BaudRate = baudrate;
USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init ( UART4, &USART_InitStructure );NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn; // we want to configure the UART4 interrupts
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; // this sets the priority group of the USART1 interrupts NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; // this sets the subpriority inside the group NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; // the UART4 interrupts are globally enabled NVIC_Init ( &NVIC_InitStructure );USART_ITConfig ( UART4, USART_IT_RXNE, ENABLE ); // RX-Data not empty IRQ
USART_Cmd ( UART4, ENABLE ); }#define RXQLEN 32 // max RX-Pufferlänge
int Uart4RxCnt; // Anzahl aktueller zeichen im RX-Puffer char Uart4RxQ[RXQLEN]; // RX-Puffervoid UART4_IRQHandler ( void )
{ while ( USART_GetITStatus ( UART4, USART_IT_RXNE ) != RESET ) { Uart4RxQ[Uart4RxCnt++] = USART_ReceiveData ( UART4 ); } }void UART4PutData ( uint16_t x )
{ USART_SendData ( USART3, x );while ( !USART_GetFlagStatus ( UART4, USART_FLAG_TXE ) );
}void UART4PutChar ( void *c )
{ USART_SendData ( UART4, * ( uint16_t * ) c );while ( !USART_GetFlagStatus ( UART4, USART_FLAG_TXE ) );
}void UART4PutString ( const char *str )
{ do { UART4PutChar ( ( void * ) str ) ; } while ( * ( uint8_t * ) str++ != '\0' ); }2015-01-18 03:13 PM
Some inconsistent use of USART3 vs UART4, and back testing of TXE rather than front testing. You want to test if a register is EMPTY before you put something in it.
2015-01-18 07:15 PM