cancel
Showing results for 
Search instead for 
Did you mean: 

PMSM FOC 4.3 debug ST-Link error

kissmucus
Associate II
Posted on December 28, 2016 at 15:38

Hi'

I have a strange problem.

I use Win 10, and Keil MDK-ARM 5.11 version

I installed the newest 4.3 PMSM foc environment, and usb driver, and firmwares.

My board is 

NUCLEO

-

F303K8 and x-nucleo-ihm07m1 expansion board

  

I can use the motor profiler, and the workbatch runs correctly.

The all kind of link works/st link/virtual com port...

I compiled the code in the keil5 without error.

But when i press the button to set the (st-link)debug link on the wizard screen,♯ the MDK-ARM is collapsed.

All other case i can set the link (example codes, own codes, different nucleo boards) except when i use 4.3 PMSM foc.

I tried to set the link with another boards but in the all cases collapsed the MDK-ARM. I think my board work well, so i have got any software/settings problem

I can do all this settings without problem in the 4.2 PMSM foc.

Can anybody help me what is my mistake?

#stm32-pmsm-foc-sdk
2 REPLIES 2
kissmucus
Associate II
Posted on January 07, 2017 at 20:58

The problem solved.

Downgrade win10 to win7 and upgrade the Mkd_arm 5.11 to 5.22 version.

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards