cancel
Showing results for 
Search instead for 
Did you mean: 

IEC60335 problem with COSMIC linker

davide239955_st
Associate II
Posted on January 26, 2015 at 17:09

Hi everybody,

I'm trying to include in my project the IEC60335 library to have class B self test. I receive this error during linker phase

#error clnk Debug\stm8slkf:1 segment .CLASS_B_REV size overflow (4)
The command: ''clnk -lC:\Programmi\COSMIC\CXSTM8_32K\Lib -o Debug\stm8ssm8 -mDebug\stm8smap Debug\stm8slkf '' has failed, the returned value is: 1
exit code=1.

I'm using STM8S105C6 micro and COSMIC compiler (32K free version). I have tried to replicate what is reported in the .lkf in the example provided with the IEC60335 library, but it doesn't work. Has anyone found this problem? Thanks #iec60335-linker-stm8s105
0 REPLIES 0