cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F469I-Discovery Audion Application is not working?

mckucukgoz
Associate II
Posted on December 17, 2015 at 09:06

I am using IAR EMBEDDED WORKBENCH 7.50.1.10273

(Common Components 7.3.1.3987)

Audio application (which is located in 

...\STM32Cube_FW_F4_V1.10.0\Projects\STM32469I Discovery\Applications\Audio\Audio_playback_and_record\EWARM) 

is not working.

When i clean and rebuild the project i get the error message :

''Fatal Error[Pe035]: #error directive: ''Reading built-in header-file. If you used upper case, try #include <stdarg.h>'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\inc\c\stdarg.h 9 ''

Can anyone help me please..

1 REPLY 1
Posted on December 22, 2015 at 16:37

Hi kucukgoz.mehmet,

 Go to this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STM32F469I-Discovery%20Audio%20application%20is%20not%20working&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&currentviews=10]Cross_post

-Shahrzad-