cancel
Showing results for 
Search instead for 
Did you mean: 

Free Development Tools: GNU ARM Eclipse

Liviu Ionescu
Associate II
Posted on August 02, 2016 at 18:05

Please add GNU ARM Eclipse, with a reference to http://gnuarmeclipse.github.io, to the list of free, open source, development environments with strong support for STM32 devices.

Regards,

Liviu

#free-development-ide-gnu-arm
19 REPLIES 19
Liviu Ionescu
Associate II
Posted on August 13, 2016 at 11:27

any moderator reading this post?

Amel NASRI
ST Employee
Posted on August 15, 2016 at 17:36

Hi Liviu Ionescu,

Thanks for your contribution in the STM32 forum. 

Do you mean to add GNU ARM Eclipse in the sticky discussion available in this forum?

I will check what can be done, if possible please provide more details on the supported devices...

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Liviu Ionescu
Associate II
Posted on August 26, 2016 at 09:37

> Do you mean to add GNU ARM Eclipse in the sticky discussion available in this forum?

yes, Mayla, please add the following:

* GNU ARM Eclipse (http://gnuarmeclipse.github.io) - supports 

all STM32 devices based on ARM Cortex-M0, M0+, M3, M4, and M7 cores. Runs on Windows, GNU/Linux and macOS. Advanced debugging features, including emulator. Completely free, completely open source.

Thank you,

Liviu

Liviu Ionescu
Associate II
Posted on September 08, 2016 at 08:18

Mayla? did you see this message?

Liviu Ionescu
Associate II
Posted on October 04, 2016 at 00:05

Mayla? Anyone else moderating this forum?

marcello2
Associate
Posted on October 05, 2016 at 10:52

I think that no one should ignore the wonderful work by Liviu Ionescu for the GNU ARM developers community.

Chapeau

Liviu Ionescu
Associate II
Posted on October 06, 2016 at 11:25

Thank you, @ferri.marcello.

Can anyone help me contact the moderators?

Liviu

AvaTar
Lead
Posted on October 06, 2016 at 13:24

There is this ''Contact moderator'' menu there:

0690X00000602czQAA.jpg

However, I would not be surprised if it didn't work ...

Liviu Ionescu
Associate II
Posted on October 10, 2016 at 18:40

> There is this ''Contact moderator'' menu 

I did this, twice, but it was of no use. :(

any other suggestions?