cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Nucleos will not install

richard239955_st
Associate
Posted on February 10, 2015 at 23:26

I just received 2 STM32L0523 board to develop When I plug them in they light up but windows does not see a USB device. I also have 2 STM32F411 board that when I plug them in Windows sees them as USB Drives, but i can not copy or save Project files  to it windows says it can not read from drive, I've tried these boards on 2 XP machines and one windows 7 Machine. Please help I want to get going with Motor Control Shield

q   
1 REPLY 1
Posted on February 11, 2015 at 05:30

Very odd. Do you have a cable problem? A hub?

Can you see the board with the ST-Link Utilities? Are the firmwares on them current?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..