2015-02-20 07:20 PM
I'm trying to get a STM32F3-Discovery to run on 72 MHz. I have a test project set up
https://github.com/sunsided/stm32f3-disco/tree/hse-problem
. The project is nothing fancy, basically a default project generated from GNU ARM Toolchain for Eclipse.However, in theSetSysClock()
code (), the loop that waits for the HSE to become ready always times out, so I'm stuck with the 8 MHz internal oscillator.I triedRCC_HSEConfig(RCC_HSE_ON)
as well asRCC_HSEConfig(RCC_HSE_Bypass)
(which I assume is what I need), to no avail. This is on a plain F3-Discovery, i.e. only the 8 MHz osc from the ST-Link, no osc on X2.Am I doing anything wrong? #stm32f3-discovery #stm32f3 #hse2015-02-20 08:48 PM
2015-02-20 09:00 PM
If I understood that correctly, SB12 should be closed, SB17 open and R33 open as well. Should be the case, this is how it looks like on my board:
R32 and R33 appear to be closed in the photo due to perspective, but are open.2015-02-21 03:52 AM
The library has code for the bypass case
STM32F3-Discovery_FW_V1.1.0\Project\Peripheral_Examples\ADC_Example\system_stm32f30x.c You might also what to check the signals with a scope, and direct the HSE signal out the MCO (PA8) pin, to see what the core sees.2015-02-21 06:36 AM
Thank you so far! The ADC example code very much looks like what I did already (and I'm glad about that! :))
I tried it nevertheless just to be sure, but it didn't work, that is, didn't change anything. As for measuring the clock via PA8, I used the following code.void
InitializeMCOGPIO() {
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure MCO (PA8) */
GPIO_InitTypeDef gpioStructure;
gpioStructure.GPIO_Pin = GPIO_Pin_8;
gpioStructure.GPIO_Speed = GPIO_Speed_50MHz;
gpioStructure.GPIO_Mode = GPIO_Mode_AF;
gpioStructure.GPIO_OType = GPIO_OType_PP;
gpioStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &gpioStructure);
/* Output HSE clock on MCO pin (PA8) */
RCC_MCOConfig(RCC_MCOSource_HSE);
}
Note that I'm unable to set a higher clock speed than
GPIO_Speed_50MHz
and my logic analyzer only samples up to 24 MHz, so I tested with several sampling rates to rule out aliasing ... without success. WithRCC_MCOSource_HSE
there's always flatline. When I useRCC_MCOSource_HSI
orRCC_MCOSource_SYSCLK
instead, I can see a wobbly, but good-enough 8 MHz waveform. So, from what it appears, the F3 doesn't even get any clock from the F103?2015-02-21 07:21 AM
Humpf ... from what it seems, the R48 resistor is dead.
EDIT: Indeed it was. I replaced the R48 resistor with one I desoldered from an old scanner board and voila, 72 MHz we go. Thanks again!