2015-02-23 06:03 AM
Hello,
I'd like to use an quadrature encoder connected to my STM32F4 Discovery Board.I have connected the A and B outputs to PC6 and PC7. CH1 and CH2 of TIM8.It works pretty good, the timer counts.Now I'd like to use the Z output of the encoder to avoid errors.I have connected Z to the CH3 of TIM8 (PC8) and configured it as an capture input.In the capture interrupt I want compare the capture value with the expected value and correct the current TIMx->CNT.Unfortunately it never enters the TIM8_CC_IRQHandler.I use this encoder:https://www.sparkfun.com/products/11102I would be very grateful if someone of you would look at my code.void configQuadratureEncoder( void ){
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7|GPIO_Pin_8; // A, B, Z; CH1, CH2, CH3 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC,GPIO_PinSource6,GPIO_AF_TIM8); GPIO_PinAFConfig(GPIOC,GPIO_PinSource7,GPIO_AF_TIM8); GPIO_PinAFConfig(GPIOC,GPIO_PinSource8,GPIO_AF_TIM8); /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 0x07ff; // Encoder -> 2048 per rotation => 0x07FF = 2047(dez) TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; // Capture Config NVIC_InitStructure.NVIC_IRQChannel = TIM8_CC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannel = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_ICInitTypeDef TIM_ICInitStructure; TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM8, &TIM_ICInitStructure); TIM_ClearITPendingBit(TIM8, TIM_IT_CC3); TIM_ITConfig(TIM8, TIM_IT_CC3, ENABLE); // END Capture Config TIM_TimeBaseInit(TIM8, &TIM_TimeBaseStructure); TIM_EncoderInterfaceConfig(TIM8, TIM_EncoderMode_TI2, TIM_ICPolarity_Falling, TIM_ICPolarity_Rising); TIM_Cmd(TIM8, ENABLE); TIM8->CNT=0; } void TIM8_CC_IRQHandler ( void ) { GPIOD->ODR ^= GPIO_Pin_12; // LED toggle GPIOD->ODR ^= GPIO_Pin_11; // Scope control if (TIM_GetITStatus(TIM8, TIM_IT_CC3) != RESET) { // correction TIM_ClearITPendingBit(TIM8, TIM_IT_CC3); } }2015-02-23 01:28 PM
2015-02-23 02:20 PM
Just checked, yes it generates a pulse. It is inverted:
The Z output is the most of the time HIGH and generates one pulse to LOW at the zero point of the encoder.I use C together with the CMSIS files.