2015-06-26 03:32 AM
Hi,
I'm trying to toggle some pins when timer 8 overflows. The problem I get is that I don´t see the pins toogle but I can see the timer counting on the debugger, so I think I might be missing some mistereous configuration on the GPIO. I'm using all 4 channels just for testing and I put a pulse value of half the timer period for testing aswell. The code I have so far:void TIM8_Init(void){
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8 ,ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_High_Speed;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC,&GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource8 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource9 ,GPIO_AF_TIM8);
TIM_TimeBaseStructure.TIM_Period = 100;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM8, &TIM_TimeBaseStructure);
//Channel 1
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Disable;
TIM_OCInitStructure.TIM_Pulse = 50;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset;
TIM_OC1Init(TIM8, &TIM_OCInitStructure);
TIM_OC2Init(TIM8, &TIM_OCInitStructure);
TIM_OC3Init(TIM8, &TIM_OCInitStructure);
TIM_OC4Init(TIM8, &TIM_OCInitStructure);
//TIM_DMACmd(TIM8, TIM_DMA_Update, ENABLE ); /* Enable TIM8_Updates DMA Requests */
//SET COUNTER
TIM8->CR1 = 0x1;
}
Thanks 🙂
2015-06-26 06:36 AM
You write:
GPIO_Init(GPIOC,&GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource8 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource9 ,GPIO_AF_TIM8);
This itches me a little. Wrong order?
First I would config the pins, then do GPIO_Init().
I use HAL, so I explicitly cannot say whether the order is right or wrong. The HAL function set all regs at once...
Have you looked in the GPIO AF reg with the debugger?
2015-06-26 06:43 AM
Not sure the pin ordering matters, provided the GPIO clock is enabled, it's pins/mux are configurable.
/* TIM8 (special) enable pins */ TIM_CtrlPWMOutputs(TIM8, ENABLE); /* TIM8 enable counter */ TIM_Cmd(TIM8, ENABLE);2015-07-01 01:57 PM
Thanks clive1!
I knew it had to be something simple that I was missing.