2015-03-09 12:39 AM
Please, confirm
my assumption: it is typing error in RM0090? Register DMA_SxFCR STM32F4xx
Bits 1:0 FTH[1:0]: FIFO threshold selection
These bits are set and cleared by software.
00: 1/4 full FIFO
01: 1/2 full FIFO
10: 3/4 full FIFO
11: full FIFO
These bits are not used in the direct mode when the DMIS value is zero.
These bits are protected and can be written only if EN is ‘1’
Must be EN = 0?P.S.
On this forum
, it is impossible to format the message
.
This is the worst
that
can be found
.
Developer
Wake up!
2015-03-09 12:58 AM
>
Must be EN = 0?
Yes. Nice catch. > P.S.On this forum
, it is impossible to format the message
.
This is the worst
that
can be found
.
Developer
Wake up!
This is a Micro$oft product and it's very unlikely ST can do anything about it. Welcome to the club. Some of the frustration can be relieved by adding a ''worst forum software ever'' tag below... 🙂 JW2015-03-09 04:59 AM
This is a Micro$oft product and it's very unlikely ST can do anything about it
.Not sure about that. Once ST had the choice, to either have a proper forum software, or something from Micro$oft. They still could migrate ... And while I don't like the above mentioned abuse NSA-bedfellow, there is more blame to put on ST. To use 'SharePoint' as user-forum software, is, euphemistically said, a little bit 'creative'.
2015-03-10 03:00 PM