cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F105 - Create USB Virtual COM port

mati
Associate
Posted on March 14, 2015 at 22:11

Hi,

I am using a Decawave EVK1000 and would like to create a USB VCOM port to my PC.

I have never made a USB driver before and have downloaded the USB FS library for the STM32F105.

From the library I see there is the Device and OTG files which I need. I See there is a VCOM example but it is for another development board.

Does anyone know of any guides or resources or at least can point me in the right direction? I want to set it up as a USB Device and output data the STM32F105 gets and pass it through USB to my PC. Do I need to use the CDC class for a VCOM?
1 REPLY 1
Dhananjay Khairnar
Associate II
Posted on March 29, 2017 at 08:42

Follow this tutuorial 

https://www.youtube.com/watch?v=tQXsUKgzSR8