cancel
Showing results for 
Search instead for 
Did you mean: 

PMSM FOC library v4.1.0 in Rowley Crossworks issue

Ond?ej Dvo?�k
Associate II
Posted on August 20, 2015 at 11:00

Hi all,

I'm using Rowley Crossword IDE for MacOS and i have issue with compiling WEB FOC v4.1.0 project (import from Keil uVision project). Always when i try to build project  i get this error: ''Can't open /PROJECT ADDRESS/BUILD CONFIGURATION/tmpdFtZGh for reading''. I used FOC v4.0 in Rowley CW and everything is OK. I checked access rights and seem's to be OK.

Do you have any idea to solution? Thanks for your help and time Ondra

   
4 REPLIES 4
prashjain007
Associate II
Posted on August 21, 2015 at 12:00

I downloaded foc support file from link given below but it is not even opening.

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257936?icmp=pf257936_pron_pr_jan2015&sc=stsw-stm32100-pr

Gigi
Senior
Posted on September 07, 2015 at 14:39

Hi

I'm sorry

We deliver the FW package with the support only for IAR and KEIL and we can't provide any help for other IDEs.

Regards

Gigi

Gigi
Senior
Posted on September 07, 2015 at 14:43

Ciao

Seems that now the link is working.

Anyhow I suggest don't trust in hyperlink and prefer to search in the ST.com the P/N of the library that will be allways: STSW-STM32100

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards