cancel
Showing results for 
Search instead for 
Did you mean: 

problem in loading the code

mukulmohalthere
Associate II
Posted on April 04, 2015 at 07:45

Hi

I was using cube for programming the stm32f030r8t6 for that there is a option of configuring the clock there I had managed clock by prescalling it to very small values i.e. /512 & /16 now when ever I used to download the code to my stm32f0 board it first shows the warning then after downloading when I used to stop the debugger then it shows error �?debugger cant be stopped this will abort the session�?. After clicking on yes it stops the debugger but then after it never download the code into the stm32f0, it shows the error

''failed to load flash loader: C:\ProgramFiles\IAR-------Flashloader\ST\flashSTM32F05xx8.h''

.then after clicking “yes�?, It shows the error “fatal error occured�?.

Now my two boards are not working with such aproblem. Please help me out. If I am doing something wrong please let me know.

1 REPLY 1
mukulmohalthere
Associate II
Posted on April 10, 2015 at 13:25

i resolved the problem of board i pressed & hold the reset button and then downloaded the program it downloaded.

but i am not getting why it happened