cancel
Showing results for 
Search instead for 
Did you mean: 

Are these appropriate LoRaWAN learning tools

Posted on December 07, 2017 at 03:29

I own a NUCLEO-L053R8.

Is it appropriate to get a I-NUCLEO-LRWAN1, plug it into the NUCLEO  and use the I-CUBE-LRWAN (STM32CubeExpansion_LRWAN_V1.1.2) to start learning LoRaWAN?

Is the NUCLEO-L053R8 with the I-NUCLEO-LRWAN1 plugged in essentially the same as a B-L072Z-LRWAN1???

14 REPLIES 14
Andrew Neil
Evangelist
Posted on December 07, 2017 at 16:21

Why risk it?

Why not just get a B-L072Z-LRWAN1 Discovery board, or a P-Nucleo-LRWAN1 kit?

http://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html

 

http://www.st.com/en/evaluation-tools/p-nucleo-lrwan1.html

 

That way, you know you have a complete kit, and you get ready-to-run examples specifically made for it - no messing about with trying to ensure that everything is compatible.

Simples!

Andrew Neil
Evangelist
Posted on December 07, 2017 at 16:28

Is the NUCLEO-L053R8 with the I-NUCLEO-LRWAN1 plugged in essentially the same as a B-L072Z-LRWAN1???

Ah - no, it isn't.

The 

I-NUCLEO-LRWAN1 has a USI module and is really just intended as a dumb modem - using AT commands:

http://www.st.com/en/evaluation-tools/i-nucleo-lrwan1.html

 

The USI module has a 

Semtech SX127

2

radio.

As noted elsewhere, the USI documentation is, well, 'lacking' ...

>:(

The Discovery board uses a muRata module with SX127

6

, and is well documented.

Note that the 

P-Nucleo-LRWAN1 kit also use the 

SX127

2

.

Posted on December 07, 2017 at 16:52

The P-NUCLEO-LRWAN1 package includes both shield and Nucleo board ($70), it is the most expensive path. You can buy the shield and board separately more cheaply. The SX1272 shield can be bought more cheaply $25, and a Nucleo for $10, but you already have that.

https://www.mouser.com/ProductDetail/Semtech/SX1272MB2DAS/?qs=5aG0NVq1C4w5nso72Adcfw%3d%3d

 

https://www.mouser.com/ProductDetail/STMicroelectronics/P-NUCLEO-LRWAN1/?qs=LtAzLad%252boeUT0TtoCWMp6w%3d%3d

 

The B-L072Z-LRWAN1 is a different beast, and perhaps the optimum development/learning platform. The L0 has 192KB of FLASH, and the module uses the SX1276 radio.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on December 07, 2017 at 16:33

The USI part can be reprogrammed, but it's a non-ideal development platform. The LRWAN that ST supplies is relatively portable across boards and platforms.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on December 07, 2017 at 16:39

Indeed - but the OP specifically asked about this as a starting point.

Of course, stuff can be ported & adapted - but I really don't think that's great as

a

starting

point.

tomkins.richard

‌ -

Turvey.Clive

‌ has postedextensively about his adventures with this stuff - including the porting across various boards...

Posted on December 07, 2017 at 16:54

Not trying to argue this point, just adding a quick footnote while I write a longer direct commentary.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on December 07, 2017 at 17:00

 ,

 ,

https://community.st.com/0D50X00009XkgY5SAJ

 ,

https://community.st.com/community/stm32-community/blog/2016/11/30/stm32-lora-kit?commentID=3505 ♯ comment-1762

 ,
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on December 07, 2017 at 17:00

Clive One wrote:

The B-L072Z-LRWAN1 is ... perhaps the optimum development/learning platform. 

I would say so.

Posted on December 08, 2017 at 01:21

I thank Clive and Andrew for the input on this question.

As a person attempting to learn something new on a limited budget, the first order of the day is to see what resources on hand can be useful in a future endeavor, hence my original question.

I had ruled out the P-NUCLEO-LRWAN1, as it is marked by ST Microelectronics as NRND, Not Recommended For New Design, indicating that it is about to be retired.

I shall go the way of your responses and acquire a

B-L072Z-LRWAN1

.