2015-04-10 09:53 AM
Hello, I have a STM32F411 nucleo board and I would like to cut STLink out. I'm building a shield for nuecleo board and I want to add a SWD connector. So I look at CN4 on STLink and altium schematic and I have some doubt about pin 1. On DM00105823.pdf say VDD_TARGET, but I can't figure out how it work on STlink 2 altium schematic. It is connected to GND throug a 10K resistor and goes nowhere (becouse there is no R9 on the board). So does anybody have a conection example for this connector?
BR2015-04-10 05:45 PM
It looks to be set up to allow for external power and measurement, ie with resistors populated or not depending on desired configuration.
1 No Connect 2 SWCLK 3 GROUND (required) 4 SWDIO 5 NRST 6 SWO (for Serial Wire Viewer) Or consider using the2015-04-10 06:44 PM
I don't know what Serial Wire Viewer is. Is this signal needed to program and debug using System Workbench? I used to use just GND, RST, SWCLK and SWDIO connections on other ARM uC. Is that ok?
This will be a shield just for me, so I don't consider the use of standar 10 pins, I need to reduce space. Thank again clive1 BR!2015-04-11 04:32 AM
It's a 0.05'' pitch header, it isn't very big.
Not familiar with System Workbench, SWV is a method of providing debug serial output, outside the normal USART type implementations. This is Keil related, but the ST-LINK Utilities also provide an SWV Console. Of course the NUCLEO boards also have a USART2/VCP configuration.