2018-01-02 10:17 AM
Hi,
Using this nucleo board, the DAC outputs only voltage from 0 to 2.1V while VDD is 3.3v.
Where's the trick?
Thanks
Julien
#dac #nucleo-f303Solved! Go to Solution.
2018-01-02 10:27 AM
2018-01-02 10:27 AM
2018-01-02 11:42 AM
Hi Clive,
Thanks for your answer.
Hum... When I connect nothing to the pin, the voltage is 0 - 3.3v.
I dived in the sheet, max current is 100 µA.
With my configuration it is 150µA...
2018-01-02 01:50 PM
when you adjust the R1 to say 33k, did you get the 3.3V you wanted ?
that works out at 97uA
I am interested to see this result.
2018-01-03 06:15 AM
I tried 75k+1k on the previous schematic : 3v....
I also tried 68k directly on the eval board with nothing else around, : 2.8v...
Julien
2018-01-04 01:11 AM
sounds like you need a 100k or a little higher, the drive must be less than 100uA