cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx Feature request : remove date / time in generated files headers or do not regenerated identical files

JulienD
Senior
Posted on May 09, 2015 at 19:41

Hi

All generated file headers are providing date/time in their headers.

When doing a re-generate code, some files are re-created exactly the same

except the generated date-time.

That's really annoying when using version control system which asks you to

commit changes while obviously there are not.

I can see two solutions for this issue ;

- remove the date-time from the file (useless when using vcs but may be usefull...)

- compare the new generated ''active code'' of the file and write on the disk only if there

are changes.

Regards

Julien

4 REPLIES 4
qwer.asdf
Senior
Posted on May 11, 2015 at 11:04

Just adding my vote for this feature.

Rob.Riggs
Senior
Posted on May 12, 2015 at 14:54

+1

jesper
Associate II
Posted on May 17, 2015 at 11:26

+1

Really annoying, makes the commits hard to navigate and hides the real changes.
Amel NASRI
ST Employee
Posted on May 19, 2015 at 18:08

Hi,

This request is already raised in

https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/BUG%20stm32cubemx%20on%20every%20save%20change%20some%20values%20randomly

. It should be implemented in next release (4.8.0).

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.