cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429I DISC - UART1 - HALDriver

felix2399
Associate
Posted on April 16, 2015 at 10:21

Hello everybody,

first i want to say that im new in the big world of microcontroller,only a basic knowledge. But now i HAVE to work with the STM32F429I-Discovery and the newest Keil uVision v5.15 and the newest CMSIS HAL Drivers.

For the beginning i want to use a Uart Port to put some Values on my Console. A simple task i thought but it will not work, there is no output in my putty but ''the driver'' returns no error.

 Can someone have a look on my Code maybe i forgot something (Enable a clock, wrong frequency , wrong pin config etc.) Some parts of the the code i create with STM32CubeMX but these porgrams do not support the ''package selection''- thing in keil so i put the config code in my keil project.

OR a different idea: can someone a keil-project where only the U(S)ART1 is enabled in asynchron and Baudrate 115200  . and send a simple ''A'' over the Pin PA9.

Code in next post:

#hal #uart #usart #stm32f429
1 REPLY 1
felix2399
Associate
Posted on April 16, 2015 at 10:36

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6nU&d=%2Fa%2F0X0000000bvg%2FY9NHg.wd_FAWInhfLoLsImeQtsFGMbjrEs54lJXEJcc&asPdf=false