2015-04-21 03:04 PM
Hi ,
As the title says, my stm32f407 gives non null values when adc pins are not connected .But , when i connect external voltage source they give reasonable values.The pins are : PC4,PC5,PA4,PA5,PA6,PA7 .This is my code :
#include ''stm32f4xx.h''
#include ''stm32f4xx_rcc.h''
#include ''stm32f4xx_gpio.h''
#include ''stm32f4xx_tim.h''
#include ''stm32f4xx_adc.h''
#include ''stm32f4xx_dma.h''
#include ''delay.h''
#include ''STM32F4-Discovery/stm32f4_discovery.h''
int
i=0;
uint16_t ADC_Val;
uint16_t ADCConvertedValue[6] = {0,0,0,0,0,0};
int
main(
void
) {
/* Initialize system */
SysTick_Init();
SystemInit();
ADC_DMA_Configuration();
while
(1) {
}
}
void
SysTick_Handler(
void
) {
TimeTick_Decrement();
}
#define ADC1_DR_Address ((uint32_t)0x4001244C)
void
ADC_DMA_Configuration(
void
) {
GPIO_InitTypeDef GPIO_InitStructure;
//Variable used to setup the GPIO pins
DMA_InitTypeDef DMA_InitStructure;
//Variable used to setup the DMA
ADC_InitTypeDef ADC_InitStructure;
//Variable used to setup the ADC
ADC_CommonInitTypeDef ADC_CommonInitStructure;
GPIO_StructInit(&GPIO_InitStructure);
ADC_StructInit(&ADC_InitStructure);
ADC_CommonStructInit(&ADC_CommonInitStructure);
DMA_StructInit(&DMA_InitStructure);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
//--Enable ADC1 and GPIOC--
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 , ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC|RCC_AHB1Periph_GPIOA, ENABLE);
GPIO_StructInit(&GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_StructInit(&GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
DMA_DeInit(DMA2_Stream4);
//Set DMA registers to default values
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
//Source address
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValue[0];
//Destination address
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 6;
//Buffer size
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
//source size - 16bit
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
// destination size = 16b
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream4, &DMA_InitStructure);
//Initialize the DMA
DMA_Cmd(DMA2_Stream4, ENABLE);
/**
Config the ADC1
*/
ADC_DeInit();
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
//continuous conversion
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_NbrOfConversion = 6;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
// 1=scan more that one channel in group
ADC_Init(ADC1,&ADC_InitStructure);
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInit(&ADC_CommonInitStructure);
//Setup order in which the Channels are sampled....
ADC_RegularChannelConfig(ADC1, ADC_Channel_4, 1, ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 2, ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC1, ADC_Channel_6, 3, ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC1, ADC_Channel_7, 4, ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 5, ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC1, ADC_Channel_15, 6, ADC_SampleTime_56Cycles);
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
ADC_DMACmd(ADC1, ENABLE);
//Enable ADC1 DMA
ADC_Cmd(ADC1, ENABLE);
//Enable ADC1
ADC_SoftwareStartConv(ADC1);
// Start ADC1 conversion
}
//end ADC_Configuration
#adc #stm32f4 #dma
2015-04-21 05:28 PM