2017-06-14 06:14 AM
I'm reading a serial ADC from an interruption (24 bits)
I need to pass its read value to the main()
I have defined in /* USER CODE BEGIN PV */ a volatile variable uint32_t xxxxx
The xxxxx variable is right inside the interruption routine but it becomes 0x01FFFFFE when called in main()
How can I pass the xxxxx variable from void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) to main()?
2017-06-14 06:18 AM
A global variable should be visible in main()
You might want another flag to indicate the presence of new data if that can't be inferred from the data itself.
2017-06-14 09:27 AM
I did as it follows
/* USER CODE BEGIN PV */
uint32_t show;volatile uint32_t measure;/* USER CODE END PV */int main(void) {
HAL_Init();
SystemClock_Config(); MX_GPIO_Init(); while (1) { show = measure; }}void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{ uint8_t i; if(GPIO_Pin== GPIO_PIN_3) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); measure = 0; for (i=0; i<24;i++) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_3)) { measure ++; } measure = measure*2; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);} else{
__NOP(); } }show and measure declared as global
measure is valid in the void
HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) scope
but become 0x1FFFFFE in main () when show = measure
Thanks
2017-06-14 09:55 AM
Probably because you're causing PA3 to bang up and down in an interrupt that triggers on PA3?
Consider using a flag to indicate if it filled the variable, or queuing the measurements, so you can see if the routine has entered multiple times.
2017-06-14 10:17 AM
I have added a new global variable variable iterac
uint8_t iterac;
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{ uint8_t i; if(GPIO_Pin== GPIO_PIN_3) { newData = 1; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);measure
= 0; for (i=0; i<24;i++) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_3)) {measure ++; }measure
=measure
*2; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); } else{ __NOP(); } iterac = i;}debugging (breakpoint at iterac = i) I see that the callback always return when iteract = 24 (that is i=24)
and measure is 0x0100033E
after 24 pulses at PA6, PA3 has been 0x0100033E. That is, there have been edges at PA3 but the interruption has only executed once.
2017-06-14 11:02 AM
>>
I see that the callback always return when iteract = 24 (that is i=24)
Well no doubt, I'm suggesting that the interrupt is reentering, not preemptively.
Make iteract a 32-bit free running counter, ie don't reset it to zero at each interrupt entry, or to the loop count.
In your main loop printf() iteract and show/measure to the SWV console.
2017-06-14 11:08 AM
Why the heck is everything being moderated today?
volatile uint32_t iterac = 0;
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{uint8_t i;iterac++; // Entry count
if(GPIO_Pin== GPIO_PIN_3) {
newData = 1;HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);measure
= 0;for (i=0; i<24;i++){HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_3)){measure ++;}measure
=measure
*2;HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);}HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);} else{__NOP();}}...
while (1) {
if (measure != 0xFFFFFFFF)
{
show = measure;
measure = 0xFFFFFFFF;
printf('%08X %08X\n', iterac, show);
}
}
2017-06-14 11:21 AM
iterac continously increasing
show and measure 0x01FFFFFE
2017-06-14 11:59 AM
2017-06-15 01:42 AM
I'm configuring the board by means STM32CubeMX
The processor is the STM32L100RC
The board is designed by me
I'm going to review the hardware. Perhaps a noise glitch in the EXTI/DataIN (PA3) is triggering the interrupt