cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubeMx stm32f2 USB_OTG_HS warning

710806594
Associate
Posted on April 27, 2015 at 07:11

when I select USB_OTG_HS->extern phy->device only peripherals, I got warning:

These IPs still have some not configured or wrong parameter values?

[Clock]

Do you still want to generate code.

what does this exactly mean? and how to solve it?

I have doing somethin wrong with cubeMx?

I have to configure some Clock manually in code?

The IPs is not stable for use?

Thanks

STM32CubeMX Version 4.7.0

Fireware Package for Family STM32F2 1.1.1

Chip: STM32F205RGTx

#usb_otg_hs
2 REPLIES 2
710806594
Associate
Posted on April 27, 2015 at 07:36

I've figured out that the clock have to be configured first.

Then, how to configure the clock with a extern phy usb?

Is their any doc or note or tutorials?

thanks

AAgha
Associate II

i have the same problem someone help please?