2015-04-27 02:38 AM
Hey together,
I'm new on STM32 Architecture (coming from god ol' AVR8) and got started with a Nucleo STM32F103RB. First steps using mbed online compiler worked so i started setting up my environment.I'm developing in Eclipse using the System Workbench Plugins and Downloaded the Cube Package by Hand from st.com.Cube Package: STM32Cube_FW_F1_V1.0.0.zipI started with the GPIO_IOToggle example from the packade, but it didn't work. After checking my toolchain 100 times, while debugging i noticed it crashed atmain() -> SystemClock_Config() -> SystemClock_Config() after the line''MODIFY_REG(RCC->CFGR, RCC_CFGR_SW, RCC_ClkInitStruct->SYSCLKSource);''(OFF TOPIC: isn't there a code tag here?)Now that uses the Define RCC_CFGR_PLLMULL16 from stm32f103xb.h, line 966:#define RCC_CFGR_PLLMULL16 ((uint32_t)0x00380000) /*!< PLL input clock*16 */Given the Reference Manual RM0008, Chapter 7.3.2, this is correct. But the µC crashes on setting the clock. So i tried to use HSI as Clock -> worked.After that i tried to use a lower PLL Multi, and PLL_MULL_8 works like a charm.Which gives me some questions:-Obvious: Why does it not work?-little strange for me:The Program calls HAL_Init before setting the clock.On HAL_Init it configures the interrupt to HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);But at that point the Controller runs on HSI which is 8MHz, after clock change it runs on HSI / 2 * 8 = 32Mhz.But my Interrupt / my HAL_Delay works fine. Why isn't it 4 times faster than expected?Im sorry if I may sound confused, I am 😉Thanks for your help, Olli