2015-04-30 04:45 PM
When system boots up, RTC is initialized and could be configured with success, but any calendar configuration afterward will always fail with '' if (RTC_EnterInitMode() == ERROR)'' in RTC_SetTime() standard API.
When system boots up, below code is called //-------------------------------------------------------------------------------void Rtc::open()
{ // Enable the Power Controller APB1 // interface clock /* Enable PWR peripheral clock */ uint32_t status; uint8_t stat = 1;RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); /* Allow access to BKP Domain */
PWR_BackupAccessCmd(ENABLE);status = RTC_ReadBackupRegister(RTC_BKP_DR19);
// Power up and wait until LSI is ready RCC_LSICmd(ENABLE); while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET) { }// Select the RTC Clock Source
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);// Enable the RTC Clock
RCC_RTCCLKCmd(ENABLE);RTC_WaitForSynchro();
//RTC_WriteBackupRegister(RTC_BKP_DR0, 0x32F2);
RTC_WriteBackupRegister(RTC_BKP_DR19, 0x1234);RTC_WaitForSynchro();
RTC_ClearITPendingBit(RTC_IT_WUT);
EXTI_ClearITPendingBit(EXTI_Line22); } //------------------------------------ Configure calendar ---------------void Rtc::write(TimeDateStruct idateTime)
{ RTC_SetTime(RTC_Format_BIN, &idateTime.time); } as you can see, RTC_SetTime is standard API from lib as below, it stops on line ''if (RTC_EnterInitMode() == ERROR)'' of ''INITF'' flag timeout. Please help this issue, thanksErrorStatus RTC_SetTime(uint32_t RTC_Format, RTC_TimeTypeDef* RTC_TimeStruct)
{ uint32_t tmpreg = 0; ErrorStatus status = ERROR; /* Check the parameters */ assert_param(IS_RTC_FORMAT(RTC_Format)); if (RTC_Format == RTC_Format_BIN) { if ((RTC->CR & RTC_CR_FMT) != (uint32_t)RESET) { assert_param(IS_RTC_HOUR12(RTC_TimeStruct->RTC_Hours)); assert_param(IS_RTC_H12(RTC_TimeStruct->RTC_H12)); } else { RTC_TimeStruct->RTC_H12 = 0x00; assert_param(IS_RTC_HOUR24(RTC_TimeStruct->RTC_Hours)); } assert_param(IS_RTC_MINUTES(RTC_TimeStruct->RTC_Minutes)); assert_param(IS_RTC_SECONDS(RTC_TimeStruct->RTC_Seconds)); } else { if ((RTC->CR & RTC_CR_FMT) != (uint32_t)RESET) { tmpreg = RTC_Bcd2ToByte(RTC_TimeStruct->RTC_Hours); assert_param(IS_RTC_HOUR12(tmpreg)); assert_param(IS_RTC_H12(RTC_TimeStruct->RTC_H12)); } else { RTC_TimeStruct->RTC_H12 = 0x00; assert_param(IS_RTC_HOUR24(RTC_Bcd2ToByte(RTC_TimeStruct->RTC_Hours))); } assert_param(IS_RTC_MINUTES(RTC_Bcd2ToByte(RTC_TimeStruct->RTC_Minutes))); assert_param(IS_RTC_SECONDS(RTC_Bcd2ToByte(RTC_TimeStruct->RTC_Seconds))); } /* Check the input parameters format */ if (RTC_Format != RTC_Format_BIN) { tmpreg = (((uint32_t)(RTC_TimeStruct->RTC_Hours) << 16) | \ ((uint32_t)(RTC_TimeStruct->RTC_Minutes) << 😎 | \ ((uint32_t)RTC_TimeStruct->RTC_Seconds) | \ ((uint32_t)(RTC_TimeStruct->RTC_H12) << 16)); } else { tmpreg = (uint32_t)(((uint32_t)RTC_ByteToBcd2(RTC_TimeStruct->RTC_Hours) << 16) | \ ((uint32_t)RTC_ByteToBcd2(RTC_TimeStruct->RTC_Minutes) << 😎 | \ ((uint32_t)RTC_ByteToBcd2(RTC_TimeStruct->RTC_Seconds)) | \ (((uint32_t)RTC_TimeStruct->RTC_H12) << 16)); }/* Disable the write protection for RTC registers */
RTC->WPR = 0xCA; RTC->WPR = 0x53;/* Set Initialization mode */
if (RTC_EnterInitMode() == ERROR) { status = ERROR; } else { /* Set the RTC_TR register */ RTC->TR = (uint32_t)(tmpreg & RTC_TR_RESERVED_MASK);/* Exit Initialization mode */
RTC_ExitInitMode();/* If RTC_CR_BYPSHAD bit = 0, wait for synchro else this check is not needed */
if ((RTC->CR & RTC_CR_BYPSHAD) == RESET) { if(RTC_WaitForSynchro() == ERROR) { status = ERROR; } else { status = SUCCESS; } } else { status = SUCCESS; } } /* Enable the write protection for RTC registers */ RTC->WPR = 0xFF; return status; }2015-04-30 06:22 PM
Make sure you reset the RTC if it gets into an unknown state, and that clocks are enabled.
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Need%20help%20initializing%20RTC%20on%20STM32F407&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=3345]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FNeed%20help%20initializing%20RTC%20on%20STM32F407&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=33452015-05-05 11:48 AM
Hello, Clivel
I did try to reset the RTC by calling ''RCC_BackupResetCmd(ENABLE); RCC_BackupResetCmd(DISABLE)'' followed when '' RTC_EnterInitMode() == ERROR'' occurred, it seemed not fix my issue at all. Is it the right way to reset RTC? the clock is sourced with LSI, with no external battery, the Vbatt is 3.3 V, I guess it is good.2016-01-14 06:12 AM
Hi xiang.sanming, I have the same problem using the HAL Library. Do you got a solution to fix this problem? Thank you!
2016-01-14 10:19 AM
I'm not sure someone who participated for 2 posts, 8 months ago, using the SPL, is going to be at all useful with your HAL issues.
See if there is anything useful you can gleen from the cited thread.