2015-05-05 04:54 AM
Hey,
I want use the SPI interface of the STM32F407 in transmit only mode. I tried some different solutions but it did not work. Can you tell me please which commands I have to use in the SPI Init? I can not find any options for transmit only in the HAL_Driver for SPI and in the header file for spi. Please help 🙂 Best regards void MX_SPI1_Init(void) { hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_1LINE; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLED; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED; hspi1.Init.CRCPolynomial = 0x1; HAL_SPI_Init(&hspi1); }2015-05-05 06:50 AM
The problem I figured out is that the HAL_SPI_Transmit function jumps into the function SPI_WaitOnFlagUntilTimeout but the TXE flag is never set to 1. The function stick in a while loop.
Can anybody help me please? The IDE I am using is Winarm (eclipse) and I am using the GCC ARM Compiler. Thanks2015-05-05 07:43 AM
Can anybody help me please?
Sorry not a HAL subscriber here. Support here is limited to those who participate.You'll need to refine ''did not work'' a bit to understand what facet didn't actually work, and which bits did.If the registers in the peripheral don't assert, make sure the clock to the peripheral is correctly enabled. If the pins don't function, check that they are clocked, correctly configured, and associated with the right peripheral.
2015-05-06 02:12 AM
Take a look to my [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F407%20discovery%20board%2c%20SPIs%20ERROR.%20Unable%20to%20get%20max%20speed%20using%20dma&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=21]post , it uses 3spis TX (but using dma).
2015-05-06 03:17 AM
Hello,
I created another project with CubeMX and now it works. I don't know where the error was. Tahnsk for reply.