cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F3xx and Ulink2 Debugger

melpel
Associate
Posted on May 20, 2015 at 17:39

Using a ULink2 debugger I can download code OK, but debugging is marginal to non-functional.  I found if I press the hardware reset AFTER entering the ''Start Debug Session'', I can usually get 1-break point to work reasonably well.  I've heard the ULink2 should use an *.ini file for proper configuration to the application, but can find no details or examples or any information which would be in that ini file.  Suggestions...?

1 REPLY 1
Posted on May 21, 2015 at 03:11

You probably want to double check you clock, pll, and flash state settings. It's going to run SystemInit() [system_stm32f3xx.c] prior to getting to your main() function, so ''run to main'' can get jammed up.

I have to use .INI files if I want to run from RAM, as you have to ''LOAD'' the executable code rather than program the FLASH. Honestly don't think ones going to help you here.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..