cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Issue: OS X and Windows version generate differing files

Craig B
Associate II
Posted on September 16, 2016 at 23:21

We recently started using the OS X version of STM32CubeMX after using the Windows version for all projects for the past 1+ years.  We found that the same .ioc file used to generate projects on the different platforms yields files that differ.  The differences I see are some spaces before CR/LF characters, especially on empty lines.  While this seems minor, the ramifications of this is that to my git clients (Tower on OS X and SourceTree on Windows), the files differ enough for them to just say the entire file has changed.  

Can you please make the OS X version output files exactly the same as those generated with the Windows version?  The Windows version seems to strip all spaces before a CR/LF.

EDIT: Sorry forgot to include the version info.

Both the OS X and Windows versions are 4.16.1

Thanks,

Craig

#stm32cubemx #generation
2 REPLIES 2
Walid FTITI_O
Senior II
Posted on September 20, 2016 at 10:29

Hi  cBroadbo,

I submit your feedback and request to our CubeMx team. I will receive response soon.

-Hannibal-
Jeanne Joly
Senior III
Posted on May 05, 2017 at 10:46

hi

Broadbooks.Craig

,

Sorry for the late answer.

It seems that there is no more issue as the one you highlighted on the lastest CubeMX releases.

So, don't hesitate to upgrade CubeMX with the latest release.

If you encounter again this issue, don't hesitate to post a new ticket on this forum.

BR. Eric