2015-11-12 05:16 AM
Hi guys.
im working on a simple encoder project where id like to read the encoder lines A and B and set a counter.although, the interruptflags on PC6 and PC7 are not beeing set and i cant see why. PC6 and 7 were tested with a oscilloscope and the signal from the encoder channels is correct. here some codingint main(void){ /* SysTick end of count event each 1ms */// RCC_GetClocksFreq(&RCC_ClockFreq);// SysTick_Config(RCC_ClockFreq.HCLK_Frequency / 1000); /* System initialization */ SysInit(); /* Endless loop */ while(1) { /* check if flags are being set */ temp--; temp = EXTI_GetFlagStatus(EXTI_Line6); temp = EXTI_GetFlagStatus(EXTI_Line7); }}void EXTI_Configuration(void){ EXTI_InitTypeDef EXTI_InitStructure; /* Connect EXTI6-8 Line to PC6-8 pin */ GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource6); GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource7); GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource8); /* Configure EXTI6-8 line */ EXTI_InitStructure.EXTI_Line = EXTI_Line6 | EXTI_Line7 | EXTI_Line8; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure);}void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /* Encoder: Configure PC6, PC7 and PC8 as input function (A,B,I) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure);}void RCC_Configuration(void){ /* Enable clock on GPIO A,B,C */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);}void NVIC_Configuration(void) { NVIC_InitTypeDef NVIC_InitStructure; #ifdef VECT_TAB_RAM /* Set the Vector Table base location at 0x20000000 */ NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); #else /* VECT_TAB_FLASH */ /* Set the Vector Table base location at 0x08000000 */ NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); #endif NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); //misc.h: NVIC_Priority_Table /* Enable and set EXTI0 Interrupt to the lowest priority */ NVIC_InitStructure.NVIC_IRQChannel = EXTI9_5_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable the USART2 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}void SysInit(void){ /* This function fills the RCC_ClockFreq structure with the current frequencies of different on chip clocks (for debug purpose) */ RCC_GetClocksFreq(&RCC_ClockFreq); /* Configure the system ticker to 1ms */ SYSTICK_Configuration(1000); /* NVIC configuration */ NVIC_Configuration(); /* System Clocks Configuration */ RCC_Configuration(); /* Configure the GPIO ports */ GPIO_Configuration(); /* Configure the USART ports */ USART_Configuration(); /* Configure Timer as Counter */ //TIM_Configuration(); /* Configure Button Interupt */ EXTI_Configuration();}void EXTI9_5_IRQHandler(void){ //if(EXTI_GetITStatus(EXTI_Line6) != RESET) //{ read_encoder(); manage_increments(); /* Clear the EXTI line pending bit */ EXTI_ClearITPendingBit(EXTI_Line6); EXTI_ClearITPendingBit(EXTI_Line7); EXTI_ClearITPendingBit(EXTI_Line8); //}}2015-11-12 05:53 AM
2015-11-12 06:01 AM
hello clive
thanks, i look into it. bunch of missing code, what else then? cant be much code missing!?2015-11-12 06:17 AM
bunch of missing code, what else then? cant be much code missing!?
It looks to be a selective cut-n-paste that won't compile. Code that does the encoder/decoder function isn't there, so hard to tell if/why that doesn't increment/decrement properly.2015-11-12 07:55 AM
Well i did not paste all the coding. but thanks a lot, its working properly now.