2015-05-29 06:14 AM
Hello all,
I want to use TIM1 and its PWM input mode to obtain duty cycle and frequency of measured signal on STM8S003. But I have uncertainty about measured value.Snippets of codevoid initialization () {//System Clocks: CLK_CKDIVR_HSIDIV = 3; // fMASTER = fHSI / 8 = 16/8 = 2MHz CLK_CKDIVR_CPUDIV = 0; // fCPU = fMASTER = 2 MHz CLK_PCKENR1_TIM1 = 1;//Timer1 TIM1_PSCRH = 0x00; TIM1_PSCRL = 0x01; // fTIM1 = fMASTER / (TIM1_PSCR + 1) = 1 MHz TIM1_CR1_UDIS = 0; TIM1_CR1_ARPE = 1; TIM1_IER_CC1IE = 1; TIM1_IER_CC2IE = 1; // Values are set according to RM0016 Reference manual, p. 169 PWM input signal measurement - Procedure TIM1_CCMR1_CC1S = 1; TIM1_CCER1_CC1P = 0; TIM1_CCMR2_CC2S = 2; TIM1_CCER1_CC2P = 1; TIM1_SMCR_TS = 5; TIM1_SMCR_SMS = 4; TIM1_CCER1_CC1E = 1; TIM1_CCER1_CC2E = 1; TIM1_CR1_CEN = 1; //start The Timer}@interrupt void PWM_vIsrHandleTimer1CaptureEvent(void) // irq12{ if(TIM1_SR1_UIF) { TIM1_SR1_UIF = 0; // never occur } if(TIM1_SR1_CC1IF) { TIM1_SR1_CC1IF = 0; // read from TIM1_CCR1L should do this dutyCycleInTicks = (TIM1_CCR1H << 😎 & 0xFF00; dutyCycleInTicks |= (TIM1_CCR1L & 0xFF); } if(TIM1_SR1_CC2IF) { TIM1_SR1_CC2IF = 0; periodInTicks = (TIM1_CCR2H << 😎 & 0xFF00; periodInTicks |= (TIM1_CCR2L & 0xFF);}Is it sufficient to use only this functions (+enable interrupt and etc) or something I am missing in work with Timers (reseting counter or?). Problem is why values are not related to input clock to TIM1. If I change TIM1_PSCRx prescaler or CLK_CKDIVR_HSIDIV (input clock to Tim1 peripheral), measured numbers are stilt the same. Generated PWM attached to TIM1_CH1 pin can vary in frequency, but value of TIM1_CCR1 is still same (4000), and TIM1_CCR2 is OK - change depends on duty cycle (for 50% it is 2000)... What am I missing?Thanks, Regards #pwm-stm82015-06-01 12:40 AM
Is there any connection to this issue?