cancel
Showing results for 
Search instead for 
Did you mean: 

Alternative Function

arunl4g
Associate II
Posted on February 18, 2016 at 09:48

Hi 

i wonder if it is possible to read the changes on the GPIO pin where the GPIO pin is configured as GPIO_Mode  = AF pin mode.  on f429?
1 REPLY 1
Posted on February 18, 2016 at 10:50

Yes.

See last point in 8.3.11 Alternate function configuration, in RM0090 rev.11.

JW