cancel
Showing results for 
Search instead for 
Did you mean: 

L3GD20 gyroscope value drift on STM32F3-Discovery

adam239955
Associate II
Posted on July 10, 2015 at 13:08

Using a D/A the converter I am now able to monitor the gyroscope rotational accelration around the x axis as a voltage.

I run the gyroscope at 190 Hz rate and read the oscilloscope in a thread every time the the DRDY interrupt gives a semaphore.

When the STM32F3-Discovery board is placed on a desk, the output is about 4500 mdps (milli degrees per second) velocity around the x axis. This is within the specified zero-rate level in the L3GD20 specification pdf, which says I can expect +- 15 dps. No surprise there.

I take 3000 samples (which takes about 15s) to get rid of the offset, but even then the D/A converter shows that the zero-rate level keeps drifting.

The L3GD20 Data Sheet doesn't say anything about a settling time, so I wonder what experiences others have had?

#l3gd20 #gyroscope #stm32f3
0 REPLIES 0