cancel
Showing results for 
Search instead for 
Did you mean: 

audio_playback_and_record example add uart2

dandantas88
Associate II
Posted on June 25, 2015 at 19:36

hello everyone.

this week i start to dev in stm32f4discovery

install cubeMX and get examples STM32Cube_FW_F4_v1.6.0

1)

at this point i want to add an uart to send the ''song'' name to be played

i added the library stm32f4xx_hal_usart.c and stm32f4xx_hal_uart.c (in any case )

and when i try to build it generate the error

''STM32F4-DISCO\STM32F4-DISCO.axf: Error: L6218E: Undefined symbol HAL_UART_Init (referred from main.o).''

because of the line 677 - see print atach

there is any point i'm missing?

2) why is no the manage run-time environment icon (green box) not active? as others projects ...

thanks in advance

grettings from Portugal

0 REPLIES 0