cancel
Showing results for 
Search instead for 
Did you mean: 

[Bug] STM32CubeMx 4.8.0 close project when i move the scrollbar

stuk
Associate II
Posted on June 17, 2015 at 14:36

Every time i move the scroolbar up or down, or left/right to resize the window, my project is closed, and i return to the startup page of the CubeMx!

0690X00000605SaQAI.png

#bug #cubemx
3 REPLIES 3
nesrine
Senior
Posted on June 17, 2015 at 16:11

Hello,

I use STM32CubeMx 4.8.0 and I don’t have such problem, if you can test this issue with another Pc

Syrine.

stuk
Associate II
Posted on June 17, 2015 at 16:20

No, i try in another pc and works well. So what's the problem? I have to reintall cubeMx?

nesrine
Senior
Posted on June 17, 2015 at 16:34

Yes,Try to reinstall CUBEMX