2015-07-01 06:53 AM
Im a newbe to arm family
Im using coocox ide.I create my 1st project compile n and downloaded to STM32F030-Discovery board.The project compiled successfully and downloaded but nothing is happening on the board.What Iam Trying is Just To Turn On The LED.Below Is My Code Pls Guide Me What Iam Missing.&sharpinclude <stm32f0xx_gpio.h>&sharpinclude <stm32f0xx_rcc.h>GPIO_InitTypeDef Gp; //Create GPIO struct//Define LED pins&sharpdefine GreenLED_Pin GPIO_Pin_9&sharpdefine BlueLED_Pin GPIO_Pin_8&sharpdefine LED_GPIO GPIOCint main(void){ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE); Gp.GPIO_Pin = GreenLED_Pin; //My alteration Gp.GPIO_Mode = GPIO_Mode_OUT; //Set GPIO pins as output Gp.GPIO_OType = GPIO_OType_PP; //Ensure output is push-pull vs open drain Gp.GPIO_PuPd = GPIO_PuPd_NOPULL; //No internal pullup resistors required Gp.GPIO_Speed = GPIO_Speed_Level_1; //Set GPIO speed to lowest GPIO_Init(LED_GPIO, &Gp); //Assign struct to LED_GPIO while(1) { GPIO_SetBits(LED_GPIO, GreenLED_Pin); }}Thank you #stm32f030r8t6-disco-beginner #keil5-stm32f030-l6320w2015-07-01 08:16 AM
2015-07-04 08:58 AM
use keil it is free for stm32f0 devices
http://www2.keil.com/stmicroelectronics-stm32/mdkand this way you benefit stm32cubemx auto code generation feature2015-07-09 04:49 AM
I got this error on keil ide while compiling
what is this Error: L6320W about ?*** Using Compiler 'V5.05 update 2 (build 169)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'Rebuild target 'Target 1'compiling Keil1.c...linking....\Objects\Keil1.axf: Error: L6320W: Ignoring --entry command. Cannot find argument 'Reset_Handler'..\Objects\Keil1.axf: Warning: L6320W: Ignoring --first command. Cannot find argument '__Vectors'.Not enough information to list image symbols.Not enough information to list the image map.Finished: 2 information, 1 warning and 1 error messages.''.\Objects\Keil1.axf'' - 1 Error(s), 1 Warning(s).Target not created.Build Time Elapsed: 00:00:022015-07-09 05:31 AM
search on google here is the link
http://www.keil.com/support/docs/3531.htmUncheck the
Use MicroLIBcheckbox in
Options for Target,
Targettab, then rebuild your project.
2015-07-09 07:49 AM
Seems more probable that the project doesn't contain a startup_stm32f0xx.s file with the vectors and startup code.
You should review the structure of the example/template projects provided with the firmware libraries.2015-07-09 08:44 AM
@aslan.mehmet
Use Microlib Is NotChecked.2015-07-09 08:50 AM
@Clive1
Actually The Error I Posted Is Shown When I Compile An Example Project.I Manually Included Directories In Options->Target -> C/C++ Tab (Keil)