cancel
Showing results for 
Search instead for 
Did you mean: 

Development Board for HFI

dwisse
Associate
Posted on July 01, 2015 at 17:24

Hello,

I was at Embedded world Germany and an Italian ST representative showed me encoderless motor control which even worked well with zero speed (using High Frequency Injection). I want to test if this works in my case. Therfor I'm looking for a good Development board which will work with HFI and preferable a Cortex microcontroller.

Which one do you recommend?

Kind Regards,

Dik-Jan

5 REPLIES 5
Gigi
Senior
Posted on September 07, 2015 at 15:30

Sorry for the delay of my answer

Probably I'm the guy you meet at EW.

For the HFI is required that you use STM32F3 or STM32F4 microcontrollers so you can use STM32F303E-EVAL or STM3241G-EVAL. Or waiting a litte more even using the Nucleo Board and adapter.

As Power Board we have a wide range of evaluation board for range of power from 100W to 2kW and you can find them in the ST.com searching for STEVAL-IHMxxx.

Ciao

Gigi

re.wolff9
Senior
Posted on January 10, 2016 at 17:31

Can HFI work with the IHM001 ?

Gigi
Senior
Posted on April 01, 2016 at 16:03

Ciao Roger

Yes, it is supported.

Ciao

Gigi

Posted on February 22, 2018 at 01:19

is the HFI algorithm limited to I-PMSM motors? 

Posted on February 26, 2018 at 04:01

yes