cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 with integrated phy

matas
Associate II
Posted on September 25, 2015 at 12:28

Hey, is there an STM32 device which would have an integrated phy and would only require an RJ45 jack for LAN interface? I tried to look for it, but I could not find it.

4 REPLIES 4
Posted on September 25, 2015 at 12:41

No.

JW
jpeacock
Associate II
Posted on September 25, 2015 at 13:56

The problem with an integrated PHY is the power required to drive the transformer coil in the connector magnetics.  The old Stellaris parts (now TI) tried this but if you look at the parts there were so many power and ground pins not much was left over for GPIO or other functions.  It looked like a great idea but didn't work so well in practice.

The other reason for an external PHY is the requirement for multiple buses.  With the right PHY the MAC port can share two or more separate Ethernet buses, important if you want redundant paths for reliable communications.

  Jack Peacock
matas
Associate II
Posted on September 28, 2015 at 09:09

Thanks for the explanation 🙂

Joerg Wagner
Senior III
Posted on December 31, 2017 at 00:06

Well, there are a bunch of microcontroller on the market with an integrated PHY. These devices have a MDI interface and just 4 lines are needed. A popular one is the W7500P.