cancel
Showing results for 
Search instead for 
Did you mean: 

Problem linking in API VL53L0x

aayala.db9
Associate II
Posted on August 15, 2016 at 17:56

I am trying to use the API for VL53L0x proximity sensor over one smt32F4Discovery developement board and I am not able to do it. The steps that I am doing are the following:

In a Keil project that it compiles and links without problem, I am adding the source file of API, these files are separated in two folder: core and platform. I have added the files of two folders to project.

After do it, I have also added related path to header file (*.h) in options for target --> C/C++ --> include paths.

After do it, I try to build target files and there are several errors, output is the following:

0690X00000603Q6QAI.jpg

There are several linking errors and I am not able to fix it.

Are there some information about how to carry the API to other platform different to x-nucleo.

Thanks in advance.

vl53l0 stm32f4

0 REPLIES 0