cancel
Showing results for 
Search instead for 
Did you mean: 

LIS331HH data rate

bognermn
Associate
Posted on July 08, 2015 at 14:00

Hello,

does anybody know how accurate the data rate of the LIS331HH sensors should be? I use two with a data rate of 1000Hz of them and want to synchronize the measurment results. For this reason i measured the Interrupt Pin INT1 of both sensors. The first one has a data rate of 995Hz and the second one has a data rate of 1000Hz. Is there a tolerance value for the data rate of these sensores?

Best regards,

max

0 REPLIES 0