cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F767 alternate function CAN3

sascha23
Associate II
Posted on April 28, 2016 at 08:31

Hi,

i want to design the mapping of my board. I need CAN3. In the STM32F767 Datasheet an unconsistency. In chapter 3 Table 10 (pin and ball definitions) is descriped that at pin PA8 the CAN3 is possible as alternate function but in table 12 (alternate function mapping) there is no CAN3 at AF11 column. What is the right information?

Thanks
1 REPLY 1
Nesrine M_O
Lead II
Posted on April 28, 2016 at 12:30

Hi neumann.sascha,

You are right. It’s a data sheet typo, the CAN3 is mapped on PA8.

Thank you for bringing this issue to our attention. It is noted and will be fixed in coming release of the document.

-Syrine-