cancel
Showing results for 
Search instead for 
Did you mean: 

Firmware package STM32F3 1.2.0 from Local with STM32CubeMX 4.8.0

sascha23
Associate II
Posted on July 10, 2015 at 14:35

Hello,

i use STM32CubeMX 4.8.0. When i try to import the Firmware package STM32F3 1.2.0 in the ''New Libraries Manager'' ''From Local...'' with the downloaded STM32CubeF3 1.2.0 i get the error message ''This package Version is not managed on this Version of STM32CubeMX''. How i can fix this Problem?
1 REPLY 1
chrif
Associate II
Posted on July 13, 2015 at 16:23

Hello Sascha,

To use the Firmware package STM32F3 1.2.0, you can download STM32CubeMX 4.9.0.It's available through this

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?s_searchtype=partnumber#

Best regards