2015-07-29 06:09 AM
Hello,
Recently I've been trying to configure writing to flash memory in STM32F3 discovery. I'm using STM32CubeMX and System Workbench for STM32. I've read many guides how to do it and example codes so I guess I already have some idea how it should work. However everywhere I look and read, people are using prepared functions like FLASH_Unlock() Lock() etc. Almost the same functions are in HAL library which I'm trying to use but I'm missing one. It is: FLASH_ClearFlag(...) My question is: does HAL libraries contain a substitute for that function (which I unfortunatelly can't find) or I just have to include a certain library to my project and if so, then what library? Regards Dominik O.2015-07-30 03:38 AM
Hello again,
I still don't know about this flag function but I managed to programm flash memory using options bytes functions. If anyone wants to learn how to get access to flash memory in STM32F3 just check this . There are many examples to various modules or devices attached to F3 discovery board and not only this one. Regards Dominik O.2015-08-05 08:10 AM
Hi oziom.dominik,
__HAL_FLASH_CLEAR_FLAG(__FLAG__) is the equivalent function of FLASH_ClearFlag(...) in HAL library. -Shahrzad-2015-08-06 06:27 AM
Thanks for the answer shahrzad. I didn't know that there are also Hall functions starting with a double floor. Now it will be much easier to find what I want 🙂