cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F0 Nucleo] Developing on Mac OS X

fredvaz7
Associate
Posted on July 19, 2015 at 23:02

Hi,

I have a Nucleo Board, STM32F072R8, and I followed this

https://stm32geek.wordpress.com/2014/10/21/stm32f3discovery-on-mac-os-x-using-eclipse-gcc-arm-and-openocd/

 to develop on Mac OS X using Eclipse IDE. Build Project it's complete but it's an error occurs when I do Debug:

target extended-remote localhost:3333

localhost:3333: Operation timed out.

monitor reset init

''monitor'' command not supported by this target.

load

You can't do that when your target is `exec'

monitor reset halt

''monitor'' command not supported by this target

Why?

But first a error occurs whit OpenOCD:  

Open On-Chip Debugger 0.9.0 (2015-05-28-12:05)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

WARNING: target/stm32f0x_stlink.cfg is deprecated, please switch to target/stm32f0x.cfg

Info : auto-selecting first available session transport ''hla_swd''. To override use 'transport select <transport>'.

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 1000 kHz

adapter_nsrst_delay: 100

none separate

srst_only separate srst_nogate srst_open_drain connect_deassert_srst

Info : Unable to match requested speed 1000 kHz, using 950 kHz

Info : Unable to match requested speed 1000 kHz, using 950 kHz

Info : clock speed 950 kHz

Error: open failed

in procedure 'init' 

in procedure 'ocd_bouncer'

Regards

#osx #stm32 #stm32f0 #stm32f072
0 REPLIES 0