2015-08-26 07:36 AM
Hi,
I want to try the USART bootloader on my nucleo board. I connected Boot0 to VDD and Boot1 to GND, I reseted the board. Then I send the command 0x7F to the board. But I have not received any response. Did I miss something? How can I know if my bootloader is corrupted? Thank you2015-08-26 09:30 AM
The chance of the boot-loader being corrupt is approaching zero, start by looking critically at what you're doing.
The device should support USART1 (PA9/PA10) and USART3 (check manual), the signalling must use EVEN PARITY, I'd suggest 9600 8E1 to start with. The signals are at CMOS levels, and are not compatible with RS232 levels without a converter. Use a terminal program like RealTerm which is capable of sending/receiving in HEX mode.2015-08-26 09:37 AM
Hi,
Please try to check the hardware resources used by this bootloader.I'd highly recommend you to refer to this about STM32 microcontroller system memory boot mode.-Syrine-2015-08-27 01:46 AM
Thank you. Indeed, I forgot the EVEN Parity.
So I configured my RealTerm as below: baud : 9600 parity: EVEN Data bits: 8 Stop Bits: 1 But, the nucleo answers 0x00... According to the diagram(AN2606): 0x7F is first checked, then it detects if there is a USB cable. But the USB cable is always plugged to supply the board. I suppose that USB cable is detected before receiving 0x7F. As there is no External Oscillator on the Board, the system resets. That's why I have received 0x00. Is it right? ________________ Attachments : Capture.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htqc&d=%2Fa%2F0X0000000aXn%2F3rrbhAAf8R1BN92vH4u_l2z1em3q_R6pNhFRWYZq0U4&asPdf=false2015-08-27 04:43 AM
The USB connection on the Nucleo doesn't connect to the F401RE, rather just the ST-LINK's F103
The 0x7F should be sent with the ''Send Numbers'' optionYou'll need to diagram/describe what you've wired up. I have ST's manuals.2015-08-27 05:14 AM
Yes I sent this with ''send numbers''
Attached a picture of my nucleo. ________________ Attachments : nucleo.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htqh&d=%2Fa%2F0X0000000aXp%2F3G.cv1HKCNw.dR7_cHpVt5MXXeigHdJ4wGcUu_G5J8w&asPdf=false2015-08-27 05:40 AM
2015-08-27 05:59 AM
Indeed, nothing is connected to USART 1. Why USART2 is not a valid path in this case?
According to the AN2606, the USART2 seems like it should be able to be used2015-08-27 08:24 AM
Actually, I changed the USART. I switched to USART1. And It is working!
Thank you clive1.2015-08-27 09:03 AM