cancel
Showing results for 
Search instead for 
Did you mean: 

VL6180x ODR

sbertuletti
Associate II
Posted on December 11, 2015 at 11:38

Hi, i don't find the output data rate in the datasheet of the VL6180x proximity sensor. I read only 10Hz in relationship with the current consumption.

What are the ODR settable ? 

Thanks

S.Bertuletti

#vl6180x #odr
1 REPLY 1
Julien NGUYEN
ST Employee
Posted on January 19, 2016 at 22:56

Hi Stephano,

The data rate is settable and depending on your application. It is done in the application layer handles by the host. You can decide the ranging rate you want. We have used 10 Hz to show the typical consumption of the device.

For example for Auto Focus assist we set it at 33 ms, because typically there are 33 frames per second, we want to have focus on each image if possible. For other applications you may not need to range so fast.

Thanks,

Julien


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.