cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube FMC Timing issue

jowen
Associate II
Posted on December 09, 2015 at 19:16

Hi

I am writing some data to an external device on the address and data bus I have used Stm32cube to set up the timing data. Once I have written the data to the device I have to strobe a data line. This is fine but the processor does not behave as I would expect. I would expect the write command to complete before the processor moves on the the next command (strobing the data line) but it appears to cache the write and continue to process the rest of the code.

So How can I ensure the write is complete (ie chip select line going high)  before the processor moves on to the next instruction. I could use a delay but there must be a way in the processor to tell it to wait or a register I can poll to see if it is complete?

Thanks

John.

Setup code

  /** Perform the SRAM2 memory initialization sequence

  */

  hsram2.Instance = FMC_NORSRAM_DEVICE;

  hsram2.Extended = FMC_NORSRAM_EXTENDED_DEVICE;

  /* hsram2.Init */

  hsram2.Init.NSBank = FMC_NORSRAM_BANK2;

  hsram2.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;

  hsram2.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;

  hsram2.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_8;

  hsram2.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;

  hsram2.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;

  hsram2.Init.WrapMode = FMC_WRAP_MODE_DISABLE;

  hsram2.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;

  hsram2.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;

  hsram2.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;

  hsram2.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;

  hsram2.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;

  hsram2.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;

  hsram2.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;

  /* Timing */

  Timing.AddressSetupTime = 15;

  Timing.AddressHoldTime = 15;

  Timing.DataSetupTime = 255;

  Timing.BusTurnAroundDuration = 15;

  Timing.CLKDivision = 16;

  Timing.DataLatency = 17;

  Timing.AccessMode = FMC_ACCESS_MODE_A;

 

  /* ExtTiming */

   HAL_SRAM_Init(&hsram2, &Timing, NULL);

#define DDS1_PIRA0      (*(volatile unsigned char*)     (0x64000000))

#define DDS1_PIRA1      (*(volatile unsigned char*)     (0x64000001))

Main code

      DDS1_PIRA0 = 0x00; // write to external device at

      DDS1_PIRA1 = 0xFF;

      HopClk2On();  // Toggle external port bit - This is being set high while the CS signal is still low - WHY

      HAL_Delay(1);

      HopClk2Off();
0 REPLIES 0