cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with terminal output

davod
Associate
Posted on August 06, 2015 at 16:54

Hello,

I have an incorrect output on the terminal, I check again it and it seems everything is ok. please help me. For clarify the case, I attached two snapshots from this situation.Also I use from linux(uclinux) of emcraft.com

https://www.emcraft.com/stm32f429discovery

Tankyou.
1 REPLY 1
Posted on August 06, 2015 at 18:11

Your primary support should come from Emcraft.

You can try other baud rates to figure out what's going on, or use a scope and determine the rate being used.

The most common failure DISCO vs EVAL boards is that the former uses an 8 MHz crystal and the latter a 25 MHz one, you need to make sure the code loaded has a coherent view of the hardware so the generated baud rates are valid.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..