cancel
Showing results for 
Search instead for 
Did you mean: 

Error in settings STM32CubeMX for LTDC on STM32F746G-Discovery?

sv1eia
Associate II
Posted on September 19, 2015 at 10:20

hi,

Trying to make an intial configuration project with CubeMX for the STM32F746G-Discovery.

When I select the board itself and instruct CubeMX to generate all board's known IPs, it places in the LTDC width and height the 640x480 pixel resolution, whereas the actual LCD according to specs is 480x272 pixel resolution.

Should we rely on the CubeMX generated code for the board?

2 REPLIES 2
Nesrine M_O
Lead II
Posted on September 28, 2015 at 18:36

Hi christos,

Thank you for your feedback. The issue has been reported internally.

-Syrine-
stm32cube-t
Senior III
Posted on March 22, 2016 at 19:40

Dear user,

Thank you for reporting this issue.

The solution is available since STM32CubeMX 4.11.

Best regards