cancel
Showing results for 
Search instead for 
Did you mean: 

Any SPDIF STM32F7 example project?

sv1eia
Associate II
Posted on August 06, 2015 at 19:30

Hi,

Searched the STM32Cube_FW_F7_V1.1.0 library but could not find an example for the SPDIF interface.

Is there any example somewhere that I could use for the SPDIF Rx connection?

Regards,

Christos

3 REPLIES 3
sv1eia
Associate II
Posted on August 14, 2015 at 20:21

I really need a sample SPDIFRX setup.

Tried the ST support but no actual details were given so far.

I just want a simple CubeMX setup guide on what values to put there.

Can someone please help me on that?

Christos

Posted on August 14, 2015 at 20:43

I guess ''simple'' is subjective, if any of this was simple, then the Reference Manual really should provide enough of the mechanics to work the hardware in software.

I'd assume the roster of talent isn't that deep, perhaps you can see if any of the

http://www.st.com/web/en/support/mcu_design_consultants.html

have specific experience in this area.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sv1eia
Associate II
Posted on August 14, 2015 at 21:24

Thanks clive but I didnt have that in mind.

Nevertheless, SPDIFRX is the interface that ST has provided ZERO examples so far, thus I do hope for ( and expect) some help regardless of 'roaster of talent'.