2016-06-01 03:28 PM
Hi,
I am trying to get STM32CubeMX + arm-gcc + Nucleo-073RZ to do things. It won't.I can see in my debugger and lst file that08000990 <SystemInit>:
SystemInit():/Users/dongfang/workspace-arm/stm32cube-playground/Nucleo073RZ_LED_Blinker/Release/../Drivers/CMSIS/Device/ST/STM32L0xx/Source/Templates/system_stm32l0xx.c:155 * @retval None */void SystemInit (void){ /*!< Set MSION bit */ RCC->CR |= (uint32_t)0x00000100; 8000990: 4b0f ldr r3, [pc, #60] ; (80009d0 <SystemInit+0x40>) 8000992: 681a ldr r2, [r3, #0] 8000994: f442 7280 orr.w r2, r2, #256 ; 0x100 8000998: 601a str r2, [r3, #0]At8000994
, the orr instruction, I get a HardFault. This surprises me! Shouldn't that instruction be supported on an L0 even if I possibly compiled for a fancier core?
How can a simple orr with an inline operand (no memory access) cause a hard fault, I don't get it..Thanks for any input!Regards, Soren2016-06-01 04:02 PM
Okay ... sorry I see it now. I realized I compiled for cortex-m3 and an orr.w got output. That thing is not supported on m0plus. Got rid of the HardFault 🙂
Regards, Soren