cancel
Showing results for 
Search instead for 
Did you mean: 

Workbench limitations

mwiesmeier9
Associate
Posted on August 26, 2015 at 09:19

Hi,

i want to run motors with Rs < 0.01 Ohm and Ld<0.010 mH (low voltage high current), but the Motor Control Workbench is limited to this values.

Can someone give me the formula to compute all the parameters from the header files, to do it by myself?

Thanks for your help

Marco

#motor-control-workbench
2 REPLIES 2
Gigi
Senior
Posted on September 07, 2015 at 14:36

Ciao Marco

It is an information that we can't deliver in this way.

I suggest to contact you nearest ST sales office.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards